Skip to main content

Will we ever have unbreakable smartphone glass? We asked an expert

smartphone glass
Image used with permission by copyright holder
Everyone drops their smartphone at some point. Even a recovered fumble triggers that unpleasant stomach lurch as visions of cracked and shattered screens run through your mind. Broken smartphone screens are the leading cause of smartphone failure and repairs can be eye-wateringly expensive – Apple charges $279 to replace the iPhone X screen, for example.

Thankfully, glass is getting tougher all the time, and one name that has become synonymous with that trend is Gorilla Glass. It has been a decade since Corning released the first version and Gorilla Glass has been used on more than 5 billion devices since then.

“The problem we set out to solve 10 years ago was to create a strengthened cover glass material that doesn’t scratch and doesn’t break,” John Bayne, vice president and general manager of Corning’s Gorilla Glass, told Digital Trends. “That’s the aspirational goal; it’s a goal we’re still focused on today, but we’ve made tremendous progress.”

Glass still breaks

Compared to the original Gorilla Glass, the most recent Gorilla Glass 5 is much stronger. If it was used in the same phone design, today’s version would allow you to drop the phone from four times higher with the same damage resistance as before. In testing Gorilla Glass 5 survived face drops from between 1.6 and 1.8 meters, which Bayne calls “selfie height,” onto 180 grit sandpaper, which replicates asphalt and concrete.

Christian de Looper/Digital Trends
Gorilla Glass 5 screen protectors in different thickness levels. Christian de Looper/Digital Trends

“Our epiphany 10 years ago was finding a way to strengthen glass by putting the surface in compression,” Bayne said.

Over the years, Corning has been able to apply higher and higher compression to protect against flaws, and if there are flaws to keep them from causing a break event. That’s good because smartphone manufacturers are employing more and more glass in the latest designs. Smartphone screens are getting bigger, frames are shrinking, and glass damage is a growing problem.

Sadly, we may not be feeling the full benefit of the improvements in strength precisely because of this shift in smartphone design. Many manufacturers want to make their devices thinner.

“They give back a little bit of the benefit of the glass by slimming it down,” Bayne explains. “It’s always a trade-off when we develop a new generation, does the phone maker want to use it all for damage resistance or do they want to use it to make a sleeker, sexier design?”

“Our epiphany 10 years ago was finding a way to strengthen glass by putting the surface in compression.”

While there’s cover glass used in smartphones is getting tougher all the time, scratches and breaks are still alarmingly common.

Solid statistics are hard to come by because we get our screens repaired in a host of different locations, from official manufacturer centers to independent repair shops. Some of us even repair them ourselves, but a surprising number of people just live with the damage.

A recent O2 survey in the U.K. found that half of all smartphone owners have damaged their screen at least once, 20 percent of Brits admitted to living with a cracked screen for more than six months, and 14 percent ended up with injuries caused by the cracked screen.

When Motorola introduced ShatterShield in 2015 it released similar survey results stating that 50 percent of people globally have experienced a cracked screen and 23 percent continued to use the phone with a broken screen.

“As good as glass is, it does still break,” Bayne said. “Glass breaks when two things happen, and this is consistent for any glass in the world throughout the history of time: There’s a flaw that’s introduced and that flaw is under tension – that’s how glass breaks.”

If you drop your phone and flip it over to find the glass intact, you count yourself lucky, but you may have already sowed the seeds of disaster. A drop onto asphalt could introduce a flaw you can’t see that leads to a break later. Keys in your pocket can also cause microscopic flaws that weaken the glass. When pressure hits, like a drop onto a hard surface, it seeks out those flaws and cracks or shatters the glass.

“We break thousands of phones in our lab intentionally to see how they break and study it,” Bayne said. “Because we have done glass for 165 years, and that’s basically what we do, we have the best glass scientists in the world here at Corning, and nobody knows more about strengthening cover glass than we do. Gorilla Glass today outperforms any other glass material you’re going to find by far.”

What about scratches?

A few years back there was talk of Apple employing sapphire glass instead of Gorilla Glass in the iPhone 6. Although sapphire offers greater scratch resistance, it’s more likely to break than Gorilla Glass when dropped. Apple stuck with Corning, but the argument about scratch versus drop damage resistance continues.

“Some things we do to the glass improve both drop and scratch resistance, but with other things you do have to make a trade-off,” Bayne said. “The number one pain point for consumers is still broken devices, so we have prioritized drop with recent generations of Gorilla Glass.”

You have this gorgeous, curved glass design that feels futuristic and the look is quickly spoiled by oily smudges.

The company does also produce Gorilla Glass SR+ which offers greater scratch resistance and is aimed primarily at the smartwatch market. It was used in the Samsung Gear S3 and Acer’s Leap Ware, and Corning continues to work with other manufacturers.

“It’s a composite material, so you get the damage resistance of Gorilla and you get scratch resistance very close to sapphire,” he said. “There are also some anti-reflective properties which manufacturers are very interested in.”

The challenge is the manufacturing process is a little more complex and so the cost of Gorilla Glass SR+ is higher. However, we may see it in smartphones in the future if Corning can drive that cost down.

Fingerprint magnets

Beyond cracks and scratches, there are some other issues with glass that can prove annoying. Anyone who owns a phone that has a glass front and back, whether it’s the LG V30, Galaxy S8, or the iPhone X, knows all about ugly fingerprints. You have this gorgeous, curved glass design that feels like the future and the look is quickly spoiled by oily smudges.

Image used with permission by copyright holder

We’ve gotten used to carrying around a microfiber cloth to polish up our phones. Corning offers an “easy to clean” (ETC) coating, usually called an oleophobic coating.

“The material repels oil, so when you do take out that cloth the oil easily wipes out. The Holy Grail there is to make it so the oil never sticks to the phone,” Bayne said. “But an effective anti-fingerprint coating has proven incredibly elusive and challenging from a technical perspective.”

Unable to prevent the marks in the first place, there is another trick that can be employed to diminish how noticeable they are.

“You can use an anti-glare treatment we call satin on the back of a glass phone,” Bayne said. “But if you use an anti-glare treatment on the high-resolution displays we use today, you end up with phenomenon called sparkle.”

The anti-glare treatment diffuses the light, reducing the effect of it being bent by oil and glass, but with displays that have resolutions higher than 200 pixels per inch (ppi), it causes bright spots to appear.

Corning has also developed an anti-microbial coating.

“We put a chemical in the glass that actually kills microbes on the surface of the glass,” Bayne said. “We’ve gotten some interest from hospitals and public displays like ATMs.”

If you’re unsure whether it’s required for phones, consider that a University of Arizona study back in 2012 found cell phones carry 10 times more bacteria than most toilet seats. More recent research examining 27 mobile phones belonging to high school students found an average of more than 17,000 bacterial gene copies per phone.

Glass screen protectors are the way to go

Returning to damage resistance, Corning continues to focus on making Gorilla Glass stronger, but if you’re worried about drop damage or scratches, then consider cases and screen protectors.

“Plastic screen protectors scratch and they don’t protect the phone from a drop, but putting on a glass screen protector if you want added protection certainly makes sense,” Bayne said.

Despite its flaws, there’s no doubt glass will continue to be a popular choice for phone makers.

Unfortunately, there’s no way to repair scratched or cracked glass, so if you do have an accident, replacement is the only way to go.

For all its flaws, glass is a great material for smartphone manufacture. It’s transparent, has a good tactile feel, it’s chemically durable, it can be shaped, it allows for a strong signal and wireless charging, and it can be treated with all sorts of useful coatings. There’s no doubt it will continue to be a popular choice for phone makers.

“Manufacturers are pursuing sleeker, thinner, more elegant designs,” Bayne said. “They’re still demanding more damage resistance in the glass, so we’ll continue to prioritize drop and damage resistance.”

Gorilla Glass 6 is still a year or so away, but it’s sure to bring a new level of durability. We may never have truly unbreakable glass, because anything can be broken under enough force, but the day when we don’t have to panic about a drop from pocket height or while we’re taking a selfie is creeping closer.

Editors' Recommendations

Simon Hill
Former Digital Trends Contributor
Simon Hill is an experienced technology journalist and editor who loves all things tech. He is currently the Associate Mobile…
Motorola’s next folding phone could be a game-changer
Moo on the Motorola Razr 40's cover screen.

Motorola Razr 50/Razr (2024) render 91Mobiles

We’ve got some exciting news about Motorola’s next lineup of foldable Razr smartphones. If the news is accurate, it could be significant for anyone about to be in the market for a new folding phone.

Read more
Best iPhone deals: Save on iPhone 15, iPhone 15 Pro Max and more
iPhone 13 Pro in blue.

The Apple iPhone is one of the most popular phone lineups on the planet, and it often places models at the top of the best phones. Its popularity can make iPhone deals difficult to find, but there are quite a few out there right now. Among them are iPhone SE deals, iPhone 14 deals, and even iPhone 15 deals, which is Apple’s most recent iPhone release. We’ve tracked down all of the best iPhone deals you can shop right now, so scroll onward if you’re looking for some great phone deals and Apple is your brand. You’ll find all of the details on how to save on an iPhone, as well as some details on which iPhone model may be right for you.
iPhone 15 128GB (AT&T) — $730, was $830 (plus up to $700 trade-in savings)

The Apple iPhone 15 finally brings with it Dynamic Island which we’ve only previously seen on the Pro range. It’s a real game changer at times and is very convenient. Alongside that, the Apple iPhone 15 has the Ceramic Shield front to keep it more protected while its 6.1-inch Super Retina XDR display promises to be up to two times brighter than the iPhone 14 in the sun. There’s also a 48MP main camera with 2x telephoto lens to help you take great shots. The A16 Bionic chip has plenty of processing power to aid with software adjustments.

Read more
Best Samsung Galaxy deals: S24, Buds, Watches and more
The Galaxy Z Fold 4's Cover Screen.

Samsung’s Galaxy lineup is made up of several different types of devices, and if you’re in the market for some savings, you’ll often find Samsung Galaxy tech among the best headphone deals, the best smartwatch deals, the best tablet deals, and the best phone deals. With so many different devices among the Galaxy lineup, and with so many Samsung Galaxy deals out there for the picking, we rounded up what we feel are the best Samsung Galaxy deals to shop right now. Reading onward you’ll find discounts on some of the best tablets, best smartwatches, and best wireless earbuds the Samsung Galaxy lineup has to offer, as well as some impressive discounts on Galaxy phones.

If you're looking for a specific type of Galaxy tech, check out Samsung Galaxy S24 deals, Samsung Galaxy Flip deals, Samsung Galaxy Fold deals, Samsung Galaxy Buds deals, and Samsung tablet deals.
Samsung Galaxy Buds 2 -- $97, was $150

Read more