CORNING, N.Y., December 9, 2014— Corning Incorporated (NYSE: GLW) announced today that Samsung has chosen 0.4 mm thick Corning® Gorilla® Glass 4 as the discrete touch cover glass in their sleekest smartphone ever – the Galaxy ALPHA.
Gorilla Glass 4 is Corning’s most damage-resistant cover glass to date and dramatically improves protection against cover glass damage during device drops. Corning reliability experts examined hundreds of broken devices to assess how and why cover glass breaks in actual use. They found that damage caused by sharp contact on the surface accounted for more than 70 percent of failures in the field. Then scientists developed test protocols to simulate these failures, and a product which could better withstand them – Gorilla Glass 4. Using 0.4 mm Gorilla Glass 4 cover glass allows device designers greater options for sleek and modern devices while maintaining remarkable damage resistance, like in the Galaxy ALPHA.
At less than 7 mm thick, the Galaxy ALPHA offers the distinctive design experience that consumers demand. Its slim profile and light weight, coupled with its durable Gorilla Glass 4 cover glass, make the Galaxy ALPHA a great fit for consumers who want a sophisticated look and feel without sacrificing functionality.
“Corning spends a great deal of time collaborating with Samsung to recommend solutions that will continually improve their device design and performance,” said Cliff Hund, general manager and president, Corning East Asia. “Device makers want to go thinner without sacrificing damage resistance. Samsung is not only meeting these requirements, but is on the cutting edge of smartphone design. The Galaxy ALPHA is the culmination of our close collaboration with Samsung.”
Gorilla Glass is the cover glass of choice for device manufacturers around the globe. Over 40 manufacturers have designed Gorilla Glass into a total of 1,395 product models, and have branded Gorilla Glass touch cover glass as a key selling feature. Since its launch in 2007, Gorilla Glass has been featured in more than 3 billion devices. For further information about Corning Gorilla Glass, please visit www.corninggorillaglass.com.
Forward-Looking and Cautionary Statements
This press release contains “forward-looking statements” (within the meaning of the Private Securities Litigation Reform Act of 1995), which are based on current expectations and assumptions about Corning’s financial results and business operations, that involve substantial risks and uncertainties that could cause actual results to differ materially. These risks and uncertainties include: the effect of global political, economic and business conditions; conditions in the financial and credit markets; currency fluctuations; tax rates; product demand and industry capacity; competition; reliance on a concentrated customer base; manufacturing efficiencies; cost reductions; availability of critical components and materials; new product commercialization; pricing fluctuations and changes in the mix of sales between premium and non-premium products; new plant start-up or restructuring costs; possible disruption in commercial activities due to terrorist activity, armed conflict, political or financial instability, natural disasters, adverse weather conditions, or major health concerns; adequacy of insurance; equity company activities; acquisition and divestiture activities; the level of excess or obsolete inventory; the rate of technology change; the ability to enforce patents; product and components performance issues; retention of key personnel; stock price fluctuations; and adverse litigation or regulatory developments. These and other risk factors are detailed in Corning’s filings with the Securities and Exchange Commission. Forward-looking statements speak only as of the day that they are made, and Corning undertakes no obligation to update them in light of new information or future events.
About Samsung Electronics Co., Ltd.
Samsung Electronics Co., Ltd. is a global leader in technology, opening new possibilities for people everywhere. Through relentless innovation and discovery, we are transforming the worlds of TVs, smartphones, tablets, PCs, cameras, home appliances, printers, LTE systems, medical devices, semiconductors and LED solutions. We employ 286,000 people across 80 countries with annual sales of US$216.7 billion. To discover more, please visit www.samsung.com.
About Corning Incorporated
Corning (www.corning.com) is one of the world’s leading innovators in materials science. For more than 160 years, Corning has applied its unparalleled expertise in specialty glass, ceramics, and optical physics to develop products that have created new industries and transformed people’s lives. Corning succeeds through sustained investment in R&D, a unique combination of material and process innovation, and close collaboration with customers to solve tough technology challenges. Corning’s businesses and markets are constantly evolving. Today, Corning’s products enable diverse industries such as consumer electronics, telecommunications, transportation, and life sciences. They include damage-resistant cover glass for smartphones and tablets; precision glass for advanced displays; optical fiber, wireless technologies, and connectivity solutions for high-speed communications networks; trusted products that accelerate drug discovery and manufacturing; and emissions-control products for cars, trucks, and off-road vehicles.
Media Relations Contact:
Anna I. Giambrone
(607) 974-5933
giambronai@corning.com
So-Young Jung
82-2-709-3446
jungsy@corning.com
Investor Relations Contact:
Ann H. S. Nicholson
(607) 974-6716
nicholsoas@corning.com